|
ARD2
1.00 for Rev B. Hardware
Airbag Reference Demonstrator using MPC5604P
|
Decision state for the ARD2 application. More...
Go to the source code of this file.
Defines | |
| #define | TRUE (1u) |
| #define | CLEAR (0u) |
| #define | BITS_IN_NIBBLE (4u) |
| #define | BITS_IN_BYTE (8u) |
| #define | BYTES_IN_16 (2u) |
| #define | BYTES_IN_32 (4u) |
| #define | BIT_DEFINITION |
| #define | BIT0 (1u << 0u) |
| #define | BIT1 (1u << 1u) |
| #define | BIT2 (1u << 2u) |
| #define | BIT3 (1u << 3u) |
| #define | BIT4 (1u << 4u) |
| #define | BIT5 (1u << 5u) |
| #define | BIT6 (1u << 6u) |
| #define | BIT7 (1u << 7u) |
| #define | BIT8 (1u << 8u) |
| #define | BIT9 (1u << 9u) |
| #define | BIT10 (1u << 10) |
| #define | BIT11 (1u << 11) |
| #define | BIT12 (1u << 12) |
| #define | BIT13 (1u << 13) |
| #define | BIT14 (1u << 14) |
| #define | BIT15 (1u << 15) |
| #define | BIT16 (1u << 16) |
| #define | BIT17 (1u << 17) |
| #define | BIT18 (1u << 18) |
| #define | BIT19 (1u << 19) |
| #define | BIT20 (1u << 20) |
| #define | BIT21 (1u << 21) |
| #define | BIT22 (1u << 22) |
| #define | BIT23 (1u << 23) |
| #define | BIT24 (1u << 24) |
| #define | BIT25 (1u << 25) |
| #define | BIT26 (1u << 26) |
| #define | BIT27 (1u << 27) |
| #define | BIT28 (1u << 28) |
| #define | BIT29 (1u << 29) |
| #define | BIT30 (1u << 30) |
| #define | BIT31 (1u << 31) |
| #define | DECISION_ERROR_SAFING_PIN BIT16 |
| #define | DECISION_ERROR_SAFING_REFERENCE BIT17 |
| #define | N_ELEMENTS(X) (sizeof(X)/sizeof(*(X))) |
Variables | |
| const uint16_t | cau16PreDecisionValidStates [] |
Decision state for the ARD2 application.
Copyright (C) 2011 Freescale Semiconductor Freescale Confidential Proprietary
History:
| const uint16_t cau16PreDecisionValidStates[] |
List of valid source states for this state